This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843ISK-ODS: "Range Bias and Rx Channel Gain/Phase Measurement and Compensation" not work in 3D People counting demo?

Part Number: IWR6843ISK-ODS

Hi all,

Have read the below threads about the calibration.

IWR6843ISK: Does 68xx_3D_people_counting support CLI: "compRangeBiasAndRxChanPhase"? - Sensors forum - Sensors - TI E2E support forums

CCS/IWR6843ISK: compRangeBiasAndRxChanPhase for 3D people counting - Sensors forum - Sensors - TI E2E support forums

May I confirm that the calibration coefficients won't work on  "3D People counting demo"?

Also, do the calibration coefficients can works in "long_range_people_detection"?

Thanks.

Tom 

  • Hello

    Allow us to confirm for each of the demo.

    Conceptually the same blocks as in the OOB demo can be applied here.  Would you help us understand if there are any specific  issues you are seeing on the existing examples that is making you consider the addition of calibration.

    Thank you,

    Vaibhav

  • Hello

    Have your tried the coefficients from the the OOBdemo and used them on the demos.

    Can you please share what has been the response from device for this.

    Thank you

    Vaibhva

  • Hi Vaibhva,

    Let me explain why we want to have calibration.

    We have a custom pcb which is the same design of the IWR6843ODS.

    However, we found that the range of radar sensing area can't reach 6m x 6m , but just  ~3m x ~3m.

    We test it with the overhead_demo_visualizer.

    We can see from the gui.

    When the target running out from the sensor ~1.5m (on both east, west, south-west, south - east direction), the target stop on this area even the target is going out further .

    Seems the FOV (field of view) can't have 60deg in our custom pcb.

    There are no this issue on the IWR6843ISK-ODS evaluation board with the same cfg file and set up.

    So, we try to do the calibration to see if we can get some improvement. 

    Thanks.

    Tom

  • Hi Team

    Do you have source code of 3D people counting Demo, if you have ,could you send it to me 

    Best regards,
    William

  • Hi Vaibhva,

    Yes, we have tried and no any output from the sensor.

    The calibration coefficients:

    compRangeBiasAndRxChanPhase 0.104491943 -0.251776984 -0.019140794 0.315451984 0.039100794 0.293860556 -0.067136508 -0.230248492 0.028963175 -0.714138413 0.16072254 0.995930317 -0.087275952 0.819209127 -0.225619365 -0.622807222 0.171797222 -0.27807 0.079231349 0.373701905 -0.084856984 0.30139254 -0.125055159 -0.235686111 0.098113254

    We copy and paste above to the chirp_configs file of overhead 3D people count demo then run the "overhead_demo_visualizer".

    After load the updated chirp_configs file, no any output from the GUI.

    If we using the below original configs, we can see that sensor works as normal and the GUI can display related point clouds and detected objects. 

    compRangeBiasAndRxChanPhase 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 

    Thanks,

    Tom

  • Hi William,

    All the source code is in the folder C:\ti\mmwave_industrial_toolbox_x_x_x.

    You can also check it in TI Resource Explorer.

    For any further questions, please create a new thread in the forum.

    As your question is not relate to the title of this thread.

    Thanks.

    Tom

  • Hello

    Based on the details provided  the issue seems to be (Please confirm):

    1. Custom PCB antenna is unable to provide the required FoV

    2. Comparison is wrt to IWR6843ISK-ODS type of antenna. (Antenna design is identical/derived from)

    3. In order to get the get matching performance you feel 'calibration'  based on Antenna will help.


    thank you,

    Vaibhav

  • Hi Vaibhav,

    1. Custom PCB antenna is unable to provide the required FoV

    Yes

    2. Comparison is wrt to IWR6843ISK-ODS type of antenna. (Antenna design is identical/derived from)

    Yes, the antenna design is identical

    3. In order to get the get matching performance you feel 'calibration'  based on Antenna will help.

    Yes, do this  'calibration'  would improve the FoV?

    Thanks.,

    Tom

  • Hello

    Thank you for confirming.

    Calibration corrects offsets in measurements,   it will not help in changing/widening/increasing the field of antenna coverage.

    THis would be an antenna design problem.

      It may be worth checking:

    1. Antenna simulation runs for expected coverage and strength

    2. Measure the actual performance for the board you have build using OOB - iterate various TX power- Rx gains combinations.

    3. Identify gaps - iterate antenna design to improve  targeted gap areas.

    There are various factors that affect the performance of antenna  spanning from design to manufacturing.

    Please see the following appnote provided on product page TI mmWave Radar sensor RF PCB Design, Manufacturing and Validation Guide

    Thank you,

    Vaibhav

  • Hi Vaibhav,

    Thanks for your information. More questions about the antenna validation.

    Calibration corrects offsets in measurements,   it will not help in changing/widening/increasing the field of antenna coverage.

    Then, what is the improvement of sensor after the offsets is corrected? Increase the accuracy of the position detection?

    THis would be an antenna design problem.

      It may be worth checking:

    1. Antenna simulation runs for expected coverage and strength

    What kind of "Antenna simulation" that we can do actually? Do TI have some tools/software set for that simulation?

    2. Measure the actual performance for the board you have build using OOB - iterate various TX power- Rx gains combinations.

    How do we know the performance using OOB? Using the web visualize and check those graphs?

    Thanks,

    Tom

  • Hello

    Calibration is accuracy/offset improvement to accommodate for system level delays and differences.

    Antenna design is a separate field. And just like HW/PCB design tools there are vendors available for this. TI has provided example  antenna's that one can reuse .  Please see the app note on manufacturing and design. 

    TI mmWave Radar sensor RF PCB Design, Manufacturing and Validation Guide

    OOB  or Raw data from the board can be used to see the  antenna radiation strength is various directions and create a plot with it.

    Thank you,

    Vaibhav