Other Parts Discussed in Thread: UNIFLASH
Hello,
I design a custom board of IWR6843AOP,I did not use CP2105; but I cannot flash it from Uart now.
I Measured the voltage of SOP PIN:
SOP2(V10) = 1.75v, SOP1(M3) = 0V, SOP0(U10)= 3.3V。
I connect the board and external XDS110 with below 3 pins:
RS232TX(U16) is connected to UARTRX of AUX 14-PIN; RS232RX(V16) is connected to UARTTX of AUX 14-PIN; and GND to GND
I can find "XDS110 Class Application/User UART"in Device Manager.
I use UniFlash to flash and configue the right port number,but it report error below: