This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DCA1000EVM: DCA1000 EVM working in CSI mode

Part Number: DCA1000EVM
Other Parts Discussed in Thread: AWR2243BOOST, AWR2243

Hi,

I would like to evaluate AWR2243BOOST in CSI mode.

Currently I am using DCA1000 EVM, which seems to support LVDS only.

Can I operate DCA1000 EVM in CSI mode ?

If not, is my only option is to connect AWR2243 directly to ECU supporting CSI (for example NVIDIA Jetson) ?

Is there any reference code for parsing the CSI packets into raw data format in the same structure as received from the DCA1000 FPGA Ethernet?

Thanks,

Ron