Other Parts Discussed in Thread: MMWAVEICBOOST,
Hi,
I am using iwr6843isk with mmwaveicboost ,and flashed the sensor platform with people_counting from industrial toolbox version 3.5 ,flashed it using uni-flash ,and using the Matlab gui was able to connect to the sensor and was able to see detection on Matlab plotting,but when i reconnect it back again ,the uart fails when config is applied ,nothing is read from the data port ,the comports come up as usual com25 and com24 ,but still not able to communicate with the board .i have to do multiple retries of reattaching the sensor to the usb port for it work again, i have two boards (iwr6843isk + mmwaveicboost) ,a new one which behaves in the same wave ,what could be going wrong, it works a 1min and when i reattach the sensor there is no response from the sensor.
please help me fix this ,going around this problem for weeks now, nothing wrong with comport drivers ,because each time they show up but only problem is there is no data on the dataport when config is applied.it doesnt work even after multiple reattaching of the sensor to the usb port .and suddenly it works.
Thanks
Rahul