This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MMWCAS-DSP-EVM: MMWCAS-DSP-EVM Power on boot problem

Part Number: MMWCAS-DSP-EVM

Hi,

Last month we bought three pcs of MMWCSA-DSP-EVM, one of them can’t work properly. We followed the guide to launch the boards, and using the same 12v 5A power supplier to launch them. Two works properly, but one could not get the right light. Here shows the result of the bad one and the good one.

Also in the TI E2E BBS has a similar problem: e2e.ti.com/support/sensors-group/sensors/f/sensors-forum/942936/mmwcas-dsp-evm-mmwcas-dsp-evm-power-on-boot-problem

Our problem is very close to theirs, and seems like the solution is to return and replace the unit. Does that mean we also need to return the bad pcs?

Thank you very much.