Hello TI team,
I'm trying to build a safety device that uses an array of ToF sensors to detect obstacles (people) and I wanted to use the OPT3101 IC.
The Requirements are:
- It must work up to 4-5m of distance;
- It must work both outdoors and indoors;
- It must detect obstacles in real time and must be able to detect objects as small as a hand/arm;
To be more precise I would like to build a ToF array of 3x2 10° emitters that point to the ground and detect objects/people. Since the OPT3101 can only manage 3 emitters, I would like to put 2 emitters in series (3x2).
Is this type of application compatible with the OPT3101 IC? Would I have problems detecting those types of obstacles? What about parts of the body such as an arm?
Thank you in advance.
Best regards