This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1843BOOST: Object detection system hardware

Part Number: AWR1843BOOST

Hi,

We are planning to create an object detection system with multiple AWR1843BOOST units.
Kindly confirm if we need these boards alone and a PC for rendering a visualizer or do we need any additional hardware?
Do we require additional Launchpad?
Regards,
Shijo Thomas
  • Hi,

    How many AWR1843BOOST EVMs do you plan to use?

    Do you plan to use the mmWave SDK demo sw ?

    The SDK demo uses uart to communicate with the PC?

    If you use multiple EVMs you need to make sure the PC will have sufficient USB ports to connect all the boards.

    No additional hardware should be needed

    thank you
    Cesar