This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843AOPEVM: Detection of metallic cables in clutter free environment

Part Number: IWR6843AOPEVM

Hi,

I am trying to do detection of thin, long objects (metallic wires ø=1-4cm) in an environment with very little clutter using the IWR6843AOPEVM board.

I would like to detect many points along each wire as this would simplify the problem. I am currently using the out-of-box demo with a configuration from demo visualizer to maximize resolution and disable peak grouping. With this setup, however, I only get a small cluster of points around the closest point on the cable. 

Do you have any suggestions to improve the number of detected points on the cables?

Thanks,
Nicolaj