Hi,
I am trying to configure the IWR6843AOPEVM board to output more detected points. More points result in greater CPU load on the device, and at some number of points the device becomes unresponse until it is reset.
Currently, I use the out-of-box firmware and the demo visualizer to do real-time tuning. As the number of points increases (e.g. by turning of peak grouping), the CPU load also increases. At some point the load is too much and I assume the device crashes.
From my short investigations it seems to be more resilient to these crashes when the selected Frame Rate (fps) in the Scene Selection is lower.
Are the crashes expected behavior? Is there something that can be changed in the visualizer or firmware to get around this behavior?
Thanks,
Nicolaj