This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2243: Unused FMCW_SYNCOUT and FMCW_CLKOUT in slave mode

Expert 7150 points
Part Number: AWR2243

Hello Vivek,

In this thread, you mentioned "The unused FM_CW_SYNCOUT/CLKOUT pins can be left unconnected  if the output is also disabled in the AWR_CHAN_CONF_SET_SB, using the "FM_CW_CLKOUT_MASTER_DIS " or " FM_CW_SYNCOUT_MASTER_DIS" parameters."

Is it the same for slave devices? Can the unused FM_CW_SYNCOUT/CLKOUT pins in slave mode be left unconnected? and Should we disable the output by using the "FM_CW_CLKOUT_SLAVE_EN" and "FM_CW_SYNCOUT_SLAVE_EN" parameters?

Best regards,
Ken