This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DCA1000EVM: DCA1000 can not connect via Set Up DCA1000 in mmWave Studio

Part Number: DCA1000EVM
Other Parts Discussed in Thread: IWR6843ISK

Hello,

I just bought the DCA1000 to learn more about my IWR6843ISK Board. 

When I start system and follow the video on the TI homepage, I can get it running until the video says to got to Set Up DCA 1000. If I want to connect the Output shows always the message time out.

I have check the setting for the static IP it is correct. I also can send a ping to the address and get a message back but still the problem with the tome out.

Any idea what I can do?