Hi ,
Customer running a pre-study using LDC1614EVM to try out a sensor solution and have noticed a changes in the standard deviation. Below is the details.
"
One of my tests was to try to decrease the frequency of the solution from about 1 MHz, achieved by using a 10nF capacitor, by switching to a 100nF capacitor. The frequency shift 1000kHz -> 385kHz was achieved, but unfortunately, the standard deviation was increased from 0.0002 to 0.0017, an increase of about 8 times.
I found the increase negative and cannot find any reason for the negative change. I see it as crucial for my design to have this understanding. Have you seen this before?
Are you able to help me sort this error out?
The setup is currently a lab-setup which very well may contain weaknesses. If weaknesses in the setup is causing the problem, I need to understand them.
"
Regards,
Maynard