Hi all,
I'm testing the level sensing lab on some large tanks and it seems like the code doesn't pick up anything greater than 20m, even when I increase the RangeLimitCfg to 200m.
RangeLimitCfg 2 1 1 200.0
Does anyone know if I can increase this range limit using the config or do I need to modify the MSS/DSS code?
Any pointers would be appreciated.
Thanks