This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843ISK-ODS: Not publishing output details

Part Number: IWR6843ISK-ODS

I am working with IWR6843ISK-ODS for people counting . My sensor launched, also when I walk front the sensor the DS2 light is blinking and not publishing any output ???  see video

How I can reduce the number of points and increasing processing time for that, which cfg exactly I need to change to do that?

Or do you have any other solution? 

Here is my cfg file, and I attached the video 

sensorStop
flushCfg
dfeDataOutputMode 1
channelCfg 15 7 0
adcCfg 2 1
adcbufCfg -1 0 1 1 1
lowPower 0 0
profileCfg 0 60.75 30.00 25.00 59.10 657930 0 54.71 1 96 2950.00 2 1 36
chirpCfg 0 0 0 0 0 0 0 1
chirpCfg 1 1 0 0 0 0 0 2
chirpCfg 2 2 0 0 0 0 0 4
frameCfg 0 2 96 0 50 1 0
dynamicRACfarCfg -1 4 4 2 4 8 16 4 4 4.00 4.50 0.50 1 1
staticRACfarCfg -1 4 4 2 4 8 16 4 6 8.00 13.00 0.30 0 0
dynamicRangeAngleCfg -1 0.75 0.0010 1 0
dynamic2DAngleCfg -1 1.5 0.0300 1 0 1 0.50 0.85 8.00
staticRangeAngleCfg -1 1 8 4
antGeometry0 0 0 -1 -1 -2 -2 -3 -3 -2 -2 -3 -3
antGeometry1 0 -1 -1 0 0 -1 -1 0 -2 -3 -3 -2
antPhaseRot 1 -1 -1 1 1 -1 -1 1 1 -1 -1 1
fovCfg -1 45.0 35.0
compRangeBiasAndRxChanPhase 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0
staticBoundaryBox -2 2 2 8.5 -2 2
boundaryBox -4.0 4.0 0.5 9 -2.0 2.0
sensorPosition 1.1 0 0
gatingParam 3 1.5 1.5 2 0
stateParam 3 3 10 40 5 600
allocationParam 200 800 0.1 15 0.5 20
maxAcceleration 0.1 0.1 0.1
trackingCfg 1 2 1000 20 67 105 50
sensorStart