This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2243: xwr2243

Part Number: AWR2243
Other Parts Discussed in Thread: TIDEP-01012, MMWCAS-RF-EVM, MMWCAS-DSP-EVM

I am using mmWave Studio 3.0.0.14 with an MMWCAS-DSP-EVM and MMWCAS-RF-EVM. For configuration, I used Cascade_Configuration_MIMO.lua. Design Guide: TIDEP-01012 shows that in MIMO mode, the max range is 150m. Does the config script, Cascade_Configuration_MIMO.lua, support that range? Or, do I have to modify the settings through mmWave Studio GUI or by updating the lua script to detect objects 100+ meters away from the RADAR?

Thanks,

Wei