Other Parts Discussed in Thread: DCA1000EVM, AWR2243,
Hi,
In continue to my previous thread:
I succeeded operating AWR2243 and DCA1000EVM in I2C functional mode (SOP7) when working with the mmwavelink example.
I now have to move to external host (Jetson Xavier), as DCA1000EVM doesn't support CSI, and I need to work with CSI data-path.
AWR2243BOOST nRESET is on.
I connected AWR2243 I2C_CLK J5 pin 17 to Jetson J30 pin 5.
I connected AWR2243 I2C_DATA J5 pin 19 to Jetson J30 pin 3.
But when running the following command:
"sudo i2cdetect -y -r 8"
No I2C address was found.
Regards,
Ron