Other Parts Discussed in Thread: DCA1000EVM
Hello,
I'm working with the AWR2243BOOST evaluation board connected to a DCA1000EVM data capture card. I've successfully configured and collected data with the mmWave Studio 2G.
I'd now like to synchronize the start of each frame with a Raspberry Pi via the GPIO pins (3.3v). My plan was to use the rising edge of the SYNC_OUT signal which I thought would be available on Pin 18 of J5. An oscope reading on that pin shows that there is no signal available there and this is confirmed by other threads in this forum.
The synchronization doesn't have to be particularly precise. Something within 1 μsec would be great, but I can tolerate up to a couple hundred μsec.
Please let me know the best way to achieve this synchronization. Other posts in this forum have suggested remapping the MCUCLK OUT signal (Pin 5 of J6) as the SYNC_OUT signal. If this is the best way to achieve this synchronization, I'll need more help in how to actually implement that while using the mmWave Studio to collect data.
Thanks in advance for any and all help!
Patrick