Other Parts Discussed in Thread: AWR1843BOOST
Hello,
We build our board using IWR1843 chip and found radiated spurious emission at around 65GHz.
The chirp setting is 76~76.25GHz and the spurious signal is around 65.76~ 66GHz as shown below.
When I shift the chirp frequency, the spurious signal changes by the same amount.
I measured with 50GHz spectrum analyzer + harmonic mixer and 110GHz UXA analyzer, the signal is same in both case.
Here are my questions.
a) I`d like to know how this frequency component comes out, please tell me possible reasons.
b) I need to eliminate this signal or at least reduce 15dB to pass certificate test. Is there any possible solutions?
I`d really appreciate it if you could give me answers or advises as soon as possible.
Best regards,
Chenglin Cui