This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP461-SP: What resistor value can be used to connect A0 and A1 pins to VCC or GND

Part Number: TMP461-SP


Hi Experts!

In space applications we typically frown on connecting signal pins directly to supply pins.

For the Address (A0 and A1) pins of the TMP461-SP what is the maximum value resistor that can be used instead of a direct connection to VCC or GND?

Also, for the float case, what resistor divider values can be used to reliably set the mid-supply level and give the corresponding proper address value. Floating pins are also generally discouraged.

Best regards,

Jim B