This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1243: mmWave cascade Radar : Index file not generated

Part Number: AWR1243
Other Parts Discussed in Thread: MMWCAS-RF-EVM

Hi, I'm using AWR1243P cascade radar (Rev C) EVM. I'm have following doubts:

1. I'm configuring the device with lua script for the aquisition of around 30s with 27272 number of frames and frame periodicity as 1.1ms. I have enabled all the tx and rx channels and transmitting one pulse per tx. While performing the transfer of file from WinSCP, I'm not able to receive the index file of each chip. I have checked in the SSD folder, but i couldn't find it there also. I made sure that there is enough space in SSD for holding the data. Can you please suggest to get the index file for each chip. (I'm using mmWave studio version 2.1.1.0 and mmwave_dfp_01_02_06_03 )

2. Is it possible to configure the virtual channel with the mmwave studio ?

3. Does the frames lost randomly? If yes how can we check, which frame is missed using mmwave studio.

Requesting your support for resolving these issues.

Thank you,

Kind Regards,

Vaishnavi Rao