Part Number: TMP117
Other Parts Discussed in Thread: STRIKE
Hi Team,
Could you help comment and solve below thermal issue case of TMP117?
Customer report a hardly issue of thermal on TMP117 in their body temp detect project.
The IC surface temperature is about 80 ℃, the current abnormally increases about 40-50mA, VDD 3.0V is normal, the I2C waveform is normal, there is no interruption of ALERT pin, and the phenomenon disappears after power-off and restart.
Note that TMP117 shares one I2C with the heart rate sensor IC.
Below is the SCH.



Thanks a lot.
William Z