This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP116: Long-distance transmission of I2C / SPI

Guru 12115 points
Part Number: TMP116

Hi,

1m harness is used to connect the TMP116 and the control board.

(1) Please teach if there are any precautions or countermeasures when routing I2C/SPI with a harness.

(2) Currently, we are considering placing a bidirectional logic level translator between the TMP116 and the control board. I would like to know if there are recommended circuits or recommended ICs for each I2C / SPI.

Thanks,

KT