In the frame Cfg of 3.4. Configuration File Format of the mmWave SDK document,
the description of frame pereiodicity states that the duty cycle must be 50% or less,
but this is because the ratio of the time when the chirp wave is ON to the frame time is 50.
Does that mean I have to keep it below 50%? Example:
Chirp frame 2.805 ms Wait time for next chirp frame 0.305 ms
Does this mean that the total time the chirp is on must be 1.405 ms?