This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1843BOOST: Setting the UART communication speed in the SDK

Part Number: AWR1843BOOST

I tried to set the UART speed in the SDK.

C: \ ti \ mmwave_sdk_03_05_00_04 \ packages \ ti \ drivers \ uart \ src
You can set the baud rate etc. from the 51st line to the 72nd line of.

Is it okay to think that the maximum baud rate setting is 921600 bps?