This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843AOP: Use CLI port to send data and Data port to receive configuration commands

Part Number: IWR6843AOP

Hello Community,

I am using IWR6843AOP and want to send more data through data port (Standard COM Port), but since data port has maximum baud rate of 921600 Mbps, I could not send more data. I observed CLI port (Enhanced COM Port) has maximum limit of 1843200 Mbps, so wanted to use this port to send data and Standard COM Port to receive commands. 

Is it possible to send Data via CLI Port and Receive configuration on Data Port ? 

Please let me know if there is any way to use UART in this configuration.

I am using IWR6843AOP for vital signs, and want to transfer more alorithm data along with vital signs and hence I need more bandwidth.

Thanks and Regards,

Neil