Hi,
Good Day. I have a customer who wants a radar kit. Please see below his query and help us if there is a device that fits for his specification. Thank you very much.
I am running a project looking at detecting the distance of an object to mm precision. The object will be about 30cm away. I understand that the radars kits you sell are usually used for a longer range than this (many meters). A lens should be able to focus the beam, but I cannot see if you sell kits with lenses that will do this.
You sell radar kits that are appropriate for (for example) automotive applications - detecting an object at a distance of 40m (for example). And you have some other information about slightly closer range radar for detecting objects closer to a vehicle. I want to see if I can use these kits (with a lens) to make measurements at a much closer distance (<1m) and at high resolution (1mm)
What I don't know is if the kits that you sell (dev boards and antenna arrays) are appropriate for mounting a lens on - and if you sell any appropriate lenses
Best Regards,
Ray Vincent