This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843AOP: Send CLI Commands over Data Port

Part Number: IWR6843AOP


Hello Community,

I am using IWR6843AOP and want to send CLI commands over Data Port. Is it possible ?

Thanks and Regards,

Neil

  • Hello

    Please  help us understand which physical port are you referring to as 'data' port?

    mmWave devices with post processing capabilities have  user/application programmable peripherals and these can be utilized for sending data out.

    Device itself has no restriction of usage of these peripherals, you have to modify/recode to get the required setup done.

    Please see the following useful links:

    Explore collateral based on context : Under ti.com/iwr  --> Design & development 

    Please see product page to understand which peripherals are available on the device:   Start at Overview  Check the device datasheet for available peripherals.

    Thank you,

    Vaibhav