Other Parts Discussed in Thread: IWR1443BOOST, , AWR1843AOP
I want to communicate and operate the demo program (or modified demo program) on the AWR1843AOPEVM and IWR1443BOOST using the 3.3V RS232 interface at any baud rate up to 5M.
This should be instead of using the USB (or Bluetooth on AWR1843AOPEVM) interface which expands to 2 serial ports on a PC.
Is it possible? and if yes, how do I do it?
On IWR1443BOOST the USB creates 2 serial ports (command and data) and the schematic shows only one RS232 interface available (AR_RS232TX and AR_RS232RX) after populating 2 DNP resistors, so how the interface will work? The firmware should be modified? or there is another RS232 port available?
Thanks