This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDEP-0091: Can not get the right distance in solid measuring environment

Part Number: TIDEP-0091
Other Parts Discussed in Thread: IWR1443BOOST, IWR1443, UNIFLASH,

Hardware: IWR1443Boost power-cycled by MSP432l Launchpad.

Software: Power Optimized Sensing Demo Software (Rec C), DEMO_CONFIG50 or DEMO_CONFIG100.

Measuring environment: Coal bunker 20 meters high。18 meters from the radar to the coal surface.

We also designed a PTFE lens for iwr1443. The diameter of the lens is 80mm, and focal length is 32mm, Beam width is 2.3° according to the  simulation

1. We can not get the right distance from the radar to the coal surface without the lens. The ehco wave is very flat, no peak.

2. We can get the right distance with the lens, but dB value is very small, the peak is not obvious for eyes.

Do we need to modify any parameter configuration for IWR1443? .Please help us.