This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDC1000: Configuring TDC1000

Part Number: TDC1000

Hello experts, 

I have started working on ultrasonic vehicle fuel level sensor. For this project i have selected the TDC1000 as AFE and C2000 as the MCU. As I understood, I have to connect my PCB to the PC in order to configure the TDC1000. I went through the TIDA 00322 reference design as well. What I wanted to know is, can I configure the TDC1000 by connecing my PCB to the PC via UART interface of the MCU? Or do I have to buy TDC1000-C2000 EVM module to configure the TDC1000 and use that configured IC in my PCB?

thank you.