This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1443: Is there operation flow for High Accuracy demo

Part Number: IWR1443


Hi community member,

I'm looking for a material about operation flow for High accuracy level sensing demo from ITB 4.8.0.
I don't find what I want a material on ITB 4.8.0.

Do you have any documents that show the process flow where the demo?

Best regards.
Cruijff

  • Hi Cruijff

    See the below flow diagram on the Zoom FFT. It is important to understand that the 1D Range FFT output is only used to determine the the three largest peaks. The three indices of these peaks are passed to the Zoom FFT block which is performed directly on to the ADC Data. If you have more questions let me know.

    Regards,

    AG