This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDEP-01012: AWR2243

Part Number: TIDEP-01012
Other Parts Discussed in Thread: AWR2243

Hi,

1.I am able to run cascade_radar_bf_demo.m in rtos mode. Now the problem is why the range-azimuth heatmap looks polar? And it's not running in realtime.

2. When I tried running cascade_radar_demo.m, the doppler graph is not looking right. Can you please explain, it's urgent

  • Hello Prashant, 

    Thankyou for reaching out. We're here to help you. 

    Can you explain your concern a little but more? What is not looking right? 

    Also, I apologize for the delay in response due to holidays here in India. We will try to get back to you as soon as possible.

    Regards,

    Ishita

  • Hi,

    Thanks for your reply. I am using processor sdk radar and rtos sd card boot for mmwave cascade dsp evm with 4 awr2243 cascade radar. I was able to boot and run the use-cases(cascade object detect demo and cascade object bf demo). MATLAB GUI application at host PC is missing some frames and the beamforming plot not running in the realtime. I can see the range - azimuth being change from polar to cartesian but it's still looking spherical.

  • Hi Prashant,

    The radar algorithms in SDK are for reference only.

    We expect customers to implement their own algorithms.

    We won't be able to provide any additional enhancement or technical support on algorithm.

    Regards,
    Stanley