Hi there,
I am currently using the MMWCAS-RF-EVM along with the MMWCAS-DSP-EVM. I was wondering if it was possible to somehow trigger a signal or a pulse of some sort (perhaps through the GPIOs) right after the first chirp/frame is fired. Could this be done in the GUI or with LUA scripts? The reason is for SAR imaging, as the chirp pulses need to be timestamped with the INS.
Your help is much appreciated.
Gabriel Gan