This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843ISK: How to set up WIFI communication between mmwave sensor and PC

Part Number: IWR6843ISK
Other Parts Discussed in Thread: IWR6843, IWR1843BOOST, , MMWAVEICBOOST, IWR1843

Hello,

 

I would like to mount the device on the wall without PC, but send tracking data from IWR6843 via WIFI module.

Can I use esp8266 (UART) to connect IWR6843 then transmit the data to PC GUI? Or do you have any recommend device for remote control?

To set up the communication between mmwave sensor and PC via WiFi, what else I need to modify in the sensor or GUI?

Thank you.

 

Regards,

Jiaqi