Other Parts Discussed in Thread: IWR1843, IWR6843AOP, , AWR1843BOOST
Hi team,
My customer is interested in IWR1843(BOOST) (and IWR6843AOP.)
They got some questions.
1. Do you have recommended measuring equipment (RF measurement)?
They used the Agilent's one but they are not sure what equipment is best for 79GHz devices.
2. Is the object data sent by UART at the bottom layer?
3. Which interface is used for the raw data such as distance, velocity and angle?
4. How are the data format for object data and object data?
5. How is the homing angle accuracy of the beam? like plus-minus x[degrees]
6. Why the receiver shifted 90 degrees compared with sender?
7. How do 2 dummy antennas work beside the receiver antenna on IWR1843BOOST?
8. How is the antenna patch like on the IWR6843AOP?
Best regards,
Yuto