What can the Contstream tab do?
It seems that you can set the output of the antenna, but can you change the output of the measurement on the sensorconfig tab, for example?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
What can the Contstream tab do?
It seems that you can set the output of the antenna, but can you change the output of the measurement on the sensorconfig tab, for example?
Hello Youskue,
Continuous streaming basically means continuous transmission of zero slope chirps (without any chirp or frame boundary) i.e. a single tone frequency. This is generally used for testing purposes.
You can use the TX output power backoff fields in the Cont Stream tab as well to vary the output power of the antenna.
Please refer to the below linked similar threads :
(+) IWR1443: Continuous Streaming Mode - Sensors forum - Sensors - TI E2E support forums
Hope this helps.
Regards,
Ishita