Other Parts Discussed in Thread: TMP61
Hello team,
1. Criteria of the resistance
D/S says resistance tolerance is +/-1% and 1.5% based on the temp range.
Note (1) says "Limits defined based on 4th order equation, tolerance will change with 'Sensor Long Term Drift' specification."
So criteria is based on below equation in the thermistor design tool?
If so, the below 4th order polynomial is guaranteed equation, right?
2. If my understanding of the above question is correct...
Below Datasheet table says minimum is 9.9kOhm and max is 10.1kOhm at 25C.
On the other hand, the resistance derived from 4th polynomial equation, it is 9959 Ohm based on the thermistor design tool.
When we look at the below table, It means 9859 Ohm is minimum and 10058 is max according to below table
.
If the resistance of 25C is 10.1kOhm, This meets R25 spec but this doesn't meet RTOL TA=25C spec.
How to think about this?
Should we think minimum is 9900Ohm and maximum is 10058Ohm to meet both spec?
3. Calibration.
Your team suggests the 1 point (room temp) calibration to enhance accuracy.
How to achieve this? Is this calibration method covered in the thermistor design tool?
Thank you.
Regards,
Hirata