This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV5013-Q1: Conducted Susceptibility Test: Is it advisable to put Output capacitors (shown in red box) on Hall sensor output PIN?

Part Number: DRV5013-Q1
Other Parts Discussed in Thread: DRV5013

Hi,

I wanted to implement two Output capacitors at the output pin of DR5013-Q1 as shown in the Figure attached. I am implementing those due to checking of Conducted susceptibility at the output pin of DRV5013 IC. Is it advisable to implement those capacitors at that point? What effect will it have on the rest of the circuit? 

Note: CHA_HALL_1 signal is going to the connector pin

Regards,

Abhi K.