Other Parts Discussed in Thread: HDC2022
I have two HDC2022EVM boards and can not connect to either of them using the online GUI or the old sensing solutions tool. I've followed the instructions and tried on 3 PCs. Windows 10 reports that it is setting up the drivers and was successful. The blue LED on the board illuminates briefly when it is plugged in, but nothing after that. I can't think of anything else I can do to better isolate the problem. Anyone have advice?
There are some other posts in the forums where the same board did not work as expected. The thread reads like the boards were identified as defective and replaced. My fear is that would involve our shipping or purchasing group, and they are not quick. If there's a way to rework / reflash the boards I want to try that first.
Thanks for any coaching, Eric