Other Parts Discussed in Thread: TMP1075
Switching from TMP1075 to TMP75. Configured device to shutdown mode, alert pin in active low and comparator mode (although not used), 1 fault and 220ms conversion rate. This way we can run the one-shot conversion rather than continuous mode. The communication looks fine at both but for some reason the TMP75 temperature reading always returns the same value. The module is connected as 8.2 TypicalApplication chapter suggests in datasheet. Supply voltage is 3.3V. The configuration has also been done to run TMP75 in continuous mode without success. This configuration also works fine on TMP1075.
I2C communication is set to 50kHz and looks like below on TMP75.
Picture 1 is setting configuration and reading it to confirm set. Picture 2 is setting one-shot. Picture 3 is reading the temperature.
pic1
.
pic2
pic3