This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPT3101: OPT3101 XTALK and PHASE CALIBRATION

Part Number: OPT3101

Dear ,

i have some questions  about Calibration (PHASE and ILL XTALK)  : 

1) OPT3101 MUST OPERATE  in CONTINUOS MODE or i can CALIBRATE in  MONO SHOT MODE ?

2) For XTALK and PHASE CALIBRATION , it is enogh the RANGE 0 ... 35 °C altough it must operate from -20 up to +40 °C  ?

       best regards

        Livio