Other Parts Discussed in Thread: , MMWAVEICBOOST
I use IWR6843 to make a board. Because LP87524 is out of stock, I use LP87523 instead of it. Another chip is used as the 3.3V voltage regulator chip.I have config the lp87523 through a MCU IIC.But I can not connect the board through JTAG or UART.
The following items have been determined,
(1)Each channel voltage is normal;
(2)The crystal work normally;
(3)The simulator work normally on IWR6843 EVM;
I test my board some pins voltage, sop0 = 3.29V, sop1 = 1.55V,sop2 = 1.55V, TMS = 2.586V,TDO = 3.29V,TDI = 2.584V,TCK = 0V;
and IWR6843 EVM board pins voltage, sop0 = 3.27V, sop1 = 1.2V,sop2 = 1.2V, TMS = 3.13V,TDO = 3.27V,TDI = 3.14V,TCK = 0V;
The attached picture is a schematics.
Can anyone answer?
Thank you.
Regards.