Other Parts Discussed in Thread: LDC0851
Thank you very much for your help.
I am trying to experiment with stacked coils using two sets of LDC_coil_EVM.
I would like to use two sets of I would like to use the LDC calculation tool to simulate if the sensing operation is possible in advance.
I would like to conduct a simulation to see if the sensing operation is possible using the LDC calculation tool.
I would like to simulate whether the sensing operation is possible using the LDC calculation tool.
The circular coil_coilH of LDC_coil_evm is used as a sensor coil: 2 layers.
When using the circular coil H of the other LDC_coil_evm as the reference coil (2 layers)
I think the total number of sensor coils and reference coils that should be input to the LDC calculation tool is '4', is that wrong?
Inquiry 2: Can you tell me how to use two sets of LDC_coil_evm stacked?
I have asked this question before, but I have not received any answer yet.
Thank you very much for your answer.