This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843ISK-ODS: Denser 3d point cloud visualization

Part Number: IWR6843ISK-ODS

this is the point cloud I generated but I would love it to be more dense 

something more like the video below

how can I make the pointcloud more dense like this

regards 

Abdullahi 

  • dfeDataOutputMode 1
    channelCfg 15 7 0
    adcCfg 2 1
    adcbufCfg -1 0 1 1 1
    lowPower 0 0
    profileCfg 0 60.75 30.00 25.00 59.10 657930 0 54.71 1 96 2950.00 2 1 36
    chirpCfg 0 0 0 0 0 0 0 3
    chirpCfg 1 1 0 0 0 0 0 3
    chirpCfg 2 2 0 0 0 0 0 4
    bpmCfg -1 1 0 1
    frameCfg 0 2 96 0 55.0 1 0
    % *************DETECTION LAYER PARAMETERS ***********************
    dynamicRangeAngleCfg -1 0.75 0.0010 1 0
    dynamicRACfarCfg -1 4 4 2 2 8 12 4 8 5 9 0.40 1 1
    dynamic2DAngleCfg -1 3 0.0300 1 0 1 0.50 0.85 8.00
    staticRangeAngleCfg -1 0 8 2
    staticRACfarCfg -1 6 2 2 2 8 8 6 4 8.00 15.00 0.30 0 0
    fineMotionCfg -1 0
    % ************* BOARD REALTED PARAMETERS ************************
    antGeometry0 0 0 -1 -1 -2 -2 -3 -3 -2 -2 -3 -3
    antGeometry1 0 -1 -1 0 0 -1 -1 0 -2 -3 -3 -2
    antPhaseRot 1 -1 -1 1 1 -1 -1 1 1 -1 -1 1
    fovCfg -1 70.0 20.0
    compRangeBiasAndRxChanPhase 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0
    % ************* TRACKING LAYER PARATMETERS **********************
    staticBoundaryBox -3 3 1 6 0 3
    boundaryBox -4 4 0 8 0 3
    sensorPosition 2 0 15
    gatingParam 3 2 2 2 4
    stateParam 3 3 6 500 5 6000
    allocationParam 40 100 0.1 20 0.5 20
    maxAcceleration 0.1 0.1 0.1
    presenceBoundaryBox -4 4 -4 4 0.5 2.5
    trackingCfg 1 2 800 30 46 96 55.0

    this is my configuration file

  • Hi Abdullahi,

    I noticed in the video filmed outside there was larger motion in a given direction compared to the indoor video where the person seemed to be walking around in a smaller area back and forth which may have lead to stronger point cloud in the outside scenario. Indoors there can also be more reflections or noise being in an enclosed space. 

    You can look at the following documentation that describes the various parameters you can change such as the SNR thresholds that can impact number of points. 

    The following snippet is from pg. 27 of the Detection Layer Parameter Tuning Guide which can be found here. 

    <mmwave_industrial_toolbox_location>/labs/people_counting/docs/3D_people_counting_detection_layer_tuning_guide.pdf

    This is another user guide dealing with tracker tuning layer that may be useful. 

    <mmwave_industrial_toolbox_location>/labs/people_counting/docs/3D_people_counting_tracker_layer_tuning_guide.pdf

    Please see the following older e2e post as well that may be related to this issue. https://e2e.ti.com/support/sensors-group/sensors/f/sensors-forum/1028114/iwr6843-point-cloud-snr-differs-depending-on-direction-of-motion/3804744?tisearch=e2e-sitesearch&keymatch=iwr6843%2520point%2520cloud%2520density#3804744

    Thanks,

    Alex Chan

  • Hello

    In order to get  more points for the object of interest you may want to:

    1. Try OOB demo for the corresponding device/board  -- This allows more flexibility in tuning the RF/Processing side of things

    2. Use the mmWave SDK User's guide  to see and modify following parameters

     - CFAR (Thresholds)

    -Static clutter

    -Mulit Object detection.

     

    To see where the above reference collateral is available please see

    MMWAVE-SDK    >>  mmwave_sdk_user_guide.pdf

    Industrial Toolbox  >>   68xx ODS - Point Cloud Demo

    Getting Up and Running with TI's mmWave Sensors

    Thank you,

    Vaibhav