This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843: Can I get Range-Doppler Heatmap or Range-Angle Heatmap by LVDS

Part Number: IWR6843

Hi, 

     I need Heatmap information, but if I use UART Rate 921600, the frame period can not keep in 50 ms.

Is the LVDS sufficient to output heatmap during 50 ms? If it is, how can I do this or this function had been provided

in SDK demo or lab.

Thanks,