This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

FDC2212: FDC2212 acquisition sensor signal background error

Part Number: FDC2212

The current formula IVD products detect the liquid level state. During the detection, a small number of products will appear in the state when no liquid is inserted at the same time, and the detected capacitance values vary greatly.The following tests were conducted:

The measurement module is energized, and the output conversion value;When the finger is removed, a small part of the product cannot return to the original value. Only when the chip is reset will it return to the initial value. The measurement waveform is shown as follows:

Schematic diagram:

Part of the code:

Hope to help point out the problem, thank you