This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP126: About TMP126 Driver code

Part Number: TMP126


I want to use MSP430 to control TMP126, single conversion, single reading and writing. The program is as follows. It doesn't work normally. The read temperature conversion result is 0xff

#ifndef _TMP126_H
#define _TMP126_H

// TMP126的端口配置

#define TMP126_SCLK_OUT P1DIR|=BIT3
#define TMP126_SCLK_0 P1OUT&=~BIT3
#define TMP126_SCLK_1 P1OUT|=BIT3

#define TMP126_CS_OUT P3DIR|=BIT1
#define TMP126_CS_0 P3OUT&=~BIT1
#define TMP126_CS_1 P3OUT|=BIT1


#define TMP126_SIO_OUT P3DIR|=BIT0
#define TMP126_SIO_IN P3DIR&=~BIT0

#define TMP126_SO_0 P3OUT&=~BIT0
#define TMP126_SO_1 P3OUT|=BIT0

#define TMP126_SI_VAL ((P3IN&BIT0)==BIT0)

#define TMP126_DATAREG 0x00
#define TMP126_STATUS 0x02
#define TMP126_CONFIGREG 0x03


#define START_TMP126 0x01
#define WAIT_TMP126_CONVERT 0x02
#define READ_TMP126_RESULT 0x03
#define IDEL_TMP126 0x04

#define SET_TMP126_CONVERT 0x012 //one-slot,62.5ms/convter


unsigned char ReadTMP126Step;
unsigned char TMP126SleepFlag;


void TMP126_port_init(void);
void spi_write_int_to_TMP126(unsigned int x);
unsigned int spi_read_int_from_TMP126(void);
void write_TMP126_reg16(unsigned char reg,unsigned int data);
unsigned int read_TMP126_reg16(unsigned char reg);
void start_TMP126(void);
float read_temperature(void);

#endif

#include "all.h"


//******************************************************************************
// @brief :
// TMP126_port_init ioport direction & int
// @note:
// none
// @para:
// none
//******************************************************************************
void TMP126_port_init(void)
{
TMP126_SCLK_OUT;
TMP126_CS_OUT;
TMP126_SIO_OUT;

}

//******************************************************************************
// @brief :
// write a int data to TMP126
// @note:
// none
// @para:
// uint_16 x data
//******************************************************************************
void spi_write_int_to_TMP126(unsigned int x)
{
for(unsigned char i=0;i<16;i++)
{
TMP126_SCLK_0;

if((x&0x8000)==0x8000)
{
TMP126_SO_1;
}
else
{
TMP126_SO_0;
}
x<<=1;

TMP126_SCLK_1;

}

}

//******************************************************************************
// @brief :
// read a int data from TMP126
// @note:
// none
// @para:
// uint_16 x data
//******************************************************************************
unsigned int spi_read_int_from_TMP126(void)
{
unsigned char x;
TMP126_SIO_IN;
TMP126_SCLK_1;

for(unsigned char i=0;i<16;i++)
{
TMP126_SCLK_0;

x<<=1;
if(TMP126_SI_VAL)
{
x|=0x01;
}
else
{
x&=~0x01;
}
TMP126_SCLK_1;

}
return x;


}
//******************************************************************************
// @brief :
// write TMP126 reg
// @note:
// none
// @para:
// uint_16 x data
//******************************************************************************
void write_TMP126_reg16(unsigned char reg,unsigned int data)
{
unsigned int temp=0;
TMP126_SIO_OUT;
temp|=reg;
spi_write_int_to_TMP126(temp);
spi_write_int_to_TMP126(data);

TMP126_SO_1;
TMP126_SIO_OUT;

}
//******************************************************************************
// @brief :
// read TMP126 reg
// @note:
// none
// @para:
// uint_16 x data
//******************************************************************************
unsigned int read_TMP126_reg16(unsigned char reg)
{
unsigned int temp=0x100;
TMP126_SIO_OUT;
temp|=reg;
spi_write_int_to_TMP126(temp);
TMP126_SIO_IN;
temp=spi_read_int_from_TMP126();
return temp;

}
//******************************************************************************
// @brief :
// start TMP126 one-shot converter
// @note:
// none
// @para:
// uint_16 x data
//******************************************************************************
void start_TMP126(void)
{
TMP126_CS_0;
write_TMP126_reg16(TMP126_CONFIGREG,SET_TMP126_CONVERT);
TMP126_CS_1;
}

//******************************************************************************
// @brief :
// read TMP126
// @note:
// none
// @para:
// uint_16 x data
//******************************************************************************
float read_temperature(void)
{
float f=-100;
unsigned int status;
INT16U x;

TMP126_CS_0;
status=read_TMP126_reg16(TMP126_STATUS);
TMP126_CS_1;

TMP126_CS_0;
x=read_TMP126_reg16(TMP126_DATAREG);
TMP126_CS_1;
if((status&BIT0)==BIT0)
{
f=(x)*0.0078125;// 0.0078125=0.03125/4
}

return f;

}

float temperatureVal;

void main (void)

{

TMP126_port_init();

while(1)

{

start_TMP126();

delay_ms(200);

temperatureVal=read_temperature();

}

}

  • Dear Xiaojun - 

    Thanks for the post and welcome to E2E! 

    Did you verify that your clock activity? Which MSP430 are you using? if you are using F5529, for example, one option with UCB0 would be:

    USB0 SPI I/O pins are P3.0, P3.1, UCB0 Chip Select is P2.3 or P2.6 and the UCB0 clock would be on P3.2.

  • I have solved my problem. This is because the CLK pin and CS pin are connected reversely when I make a PCB

  • #ifndef _TMP126_H
    #define _TMP126_H

    // TMP126的端口配置

    #define TMP126_SCLK_OUT P1DIR|=BIT3
    #define TMP126_SCLK_0 P1OUT&=~BIT3
    #define TMP126_SCLK_1 P1OUT|=BIT3

    #define TMP126_CS_OUT P3DIR|=BIT1
    #define TMP126_CS_0 P3OUT&=~BIT1
    #define TMP126_CS_1 P3OUT|=BIT1


    #define TMP126_SIO_OUT P3DIR|=BIT0
    #define TMP126_SIO_IN P3DIR&=~BIT0

    #define TMP126_SO_0 P3OUT&=~BIT0
    #define TMP126_SO_1 P3OUT|=BIT0

    #define TMP126_SI_VAL ((P3IN&BIT0)==BIT0)

    #define TMP126_DATAREG 0x00
    #define TMP126_STATUS 0x02
    #define TMP126_CONFIGREG 0x03


    #define START_TMP126 0x01
    #define WAIT_TMP126_CONVERT 0x02
    #define READ_TMP126_RESULT 0x03
    #define IDEL_TMP126 0x04

    #define SET_TMP126_CONVERT 0x012 //one-slot,62.5ms/convter


    unsigned char ReadTMP126Step;
    unsigned char TMP126SleepFlag;


    void TMP126_port_init(void);
    void spi_write_int_to_TMP126(unsigned int x);
    unsigned int spi_read_int_from_TMP126(void);
    void write_TMP126_reg16(unsigned char reg,unsigned int data);
    unsigned int read_TMP126_reg16(unsigned char reg);
    void start_TMP126(void);
    float read_temperature(void);

    #endif

    #include "all.h"


    //******************************************************************************
    // @brief :
    // TMP126_port_init ioport direction & int
    // @note:
    // none
    // @para:
    // none
    //******************************************************************************
    void TMP126_port_init(void)
    {
    TMP126_SCLK_OUT;
    TMP126_CS_OUT;
    TMP126_SIO_OUT;

    }

    //******************************************************************************
    // @brief :
    // write a int data to TMP126
    // @note:
    // none
    // @para:
    // uint_16 x data
    //******************************************************************************
    void spi_write_int_to_TMP126(unsigned int x)
    {
    for(unsigned char i=0;i<16;i++)
    {
    TMP126_SCLK_0;

    if((x&0x8000)==0x8000)
    {
    TMP126_SO_1;
    }
    else
    {
    TMP126_SO_0;
    }
    x<<=1;

    TMP126_SCLK_1;

    }

    }

    //******************************************************************************
    // @brief :
    // read a int data from TMP126
    // @note:
    // none
    // @para:
    // uint_16 x data
    //******************************************************************************
    unsigned int spi_read_int_from_TMP126(void)
    {
    unsigned int x;
    TMP126_SIO_IN;
    TMP126_SCLK_1;

    for(unsigned char i=0;i<16;i++)
    {
    TMP126_SCLK_0;

    x<<=1;
    if(TMP126_SI_VAL)
    {
    x|=0x01;
    }
    else
    {
    x&=~0x01;
    }
    TMP126_SCLK_1;

    }
    return x;


    }
    //******************************************************************************
    // @brief :
    // write TMP126 reg
    // @note:
    // none
    // @para:
    // uint_16 x data
    //******************************************************************************
    void write_TMP126_reg16(unsigned char reg,unsigned int data)
    {
    unsigned int temp=0;
    TMP126_SIO_OUT;
    temp|=reg;
    spi_write_int_to_TMP126(temp);
    spi_write_int_to_TMP126(data);

    TMP126_SO_1;
    TMP126_SIO_OUT;

    }
    //******************************************************************************
    // @brief :
    // read TMP126 reg
    // @note:
    // none
    // @para:
    // uint_16 x data
    //******************************************************************************
    unsigned int read_TMP126_reg16(unsigned char reg)
    {
    unsigned int temp=0x100;
    TMP126_SIO_OUT;
    temp|=reg;
    spi_write_int_to_TMP126(temp);
    TMP126_SIO_IN;
    temp=spi_read_int_from_TMP126();
    return temp;

    }
    //******************************************************************************
    // @brief :
    // start TMP126 one-shot converter
    // @note:
    // none
    // @para:
    // uint_16 x data
    //******************************************************************************
    void start_TMP126(void)
    {
    TMP126_CS_0;
    write_TMP126_reg16(TMP126_CONFIGREG,SET_TMP126_CONVERT);
    TMP126_CS_1;
    }

    //******************************************************************************
    // @brief :
    // read TMP126
    // @note:
    // none
    // @para:
    // uint_16 x data
    //******************************************************************************
    float read_temperature(void)
    {
    float f=-100;
    unsigned int status;
    INT16U x;

    TMP126_CS_0;
    status=read_TMP126_reg16(TMP126_STATUS);
    TMP126_CS_1;

    TMP126_CS_0;
    x=read_TMP126_reg16(TMP126_DATAREG);
    TMP126_CS_1;
    if((status&BIT0)==BIT0)
    {
    f=(x)*0.0078125;// 0.0078125=0.03125/4
    }

    return f;

    }

    float temperatureVal;

    void main (void)

    {

    TMP126_port_init();

    while(1)

    {

    start_TMP126();

    delay_ms(200);

    temperatureVal=read_temperature();

    }

    }

  • Dear Xiaojun - 

    Thanks for the follow-up, glad that fixed your issue.