Other Parts Discussed in Thread: MMWCAS-DSP-EVM, TIDEP-01012, TDA2
Hi,
I am using the TI AWR1243P Cascade Radar evaluation board (TIDEP-01012) with the TI MMWCAS-DSP-EVM Evaluation module (TIDEP-01017).
I tried both the MIMO script and the TxBF lua script and the postprocessing files that are in the Matlab examples.
A picture of the setup is below: I am looking at a metallic plaque which is at about 4m away.
Below are the results I obtain with both scripts.
The range azimuth heatmaps show some blobs but with very low contrast, do you know what could be the reason for it?
The range profile seems to indicate that I have a very high background signal at about 100dB, is that correct?
Thank you very much,
With the TxBF script
With the MIMO script
Picture of the setup