Hello,
I have just received my AWR2944EVM.
1. I have installed mmwave_mcuplus_sdk_04_02_00_01
2. I have installed TI CloudAgent Bridge
3.after connected the power supplier ( 12V, Max 5A) and the usb cable into XDS_USB port
I can find the XDS110 Class Application/User UART(COM3), XDS110 Class Auxiliary Data Port (Com4)
in MMWAVE-DEMO-VISUALIZER-CLOUD 4.2, I can also see the two ports
but connecting is not working.
I have tried different PC, same issues
System Windows 10 Professional
Need help!!!
Thanks
YI