This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843ISK: Pin description for SOP control over 60-pin HD connector

Part Number: IWR6843ISK
Other Parts Discussed in Thread: IWR6843

In the datasheet, it is mentioned that pin numbers 17, 24 and 49 correspond to the SOPs 0,1 and 2 in the 60-pin HD connector of the IWR6843ISK. However, they are muxed with other signals on those pins. What is the mux select pin for those 3 SOPs? Also, pin 12 is mentioned as NRST, is that equivalent to the physical Reset switch on the board?